2508_Wiser_KNX

Before You Install the Mobile Application

After meeting the following requirements, you can start installing and setting up your mobile application:

Running KNX installation

A system integrator or electrician installed and set up the KNX devices using the ETS application or Schneider´s eConfigure commissioning tool.

Wiser for KNX controller installed

The controller fulfills the hardware and firmware requirements in chapter Prepare Your Controller. It has been properly set up, the KNX project has been imported into it.

The controller properly set up, the KNX project imported into the controller

For detailed information, refer to the Wiser for KNX user guide, which is available at https://www.productinfo.schneider-electric.com/w4k_sl_ug/.

Touch visualization created

See more in Touch 3 Visualization.

  • Touch 3 is a widget-based visualization that provides easy control over KNX and Zigbee devices in the installation.

    In a few steps, the system integrator creates the building structure (floor and rooms), adds specific widgets and selects the required KNX group objects depending on the widget´s function.

    Once created, widgets will automatically generate the visualization in the Wiser KNX app.

    You can add widgets at any time later. Widgets are automatically synchronized with the Wiser KNX app.

    For detailed information on how to create the visualization in Touch and configure the widgets, refer to the instruction Wiser for KNX, SpaceLYnk - How to create a widget-based visualization in Touch 3 available here: https://www.se.com/ww/en/download/document/AN002_105_SL/.



  • eConfigure is the software tool for designing, configuring, and maintaining the KNX building automation system. With this tool, you can manage your KNX installation without perfect knowledge of KNX or ETS. See more here.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.