2508_Wiser_KNX

KOSTAL Plenticore

A Modbus profile is available for this model of an inverter: KOSTAL-Plenticore.json.

The following registers shall be mapped to KNX objects from the profile (battery registers shall be mapped only if a battery is available):

Modbus register

Modbus address

Designation

Total Active Power (power meter)

252

Grid: Active power

Total Home Consumption Grid

112

Grid: Active energy produced by the grid (energy taken by house)

Total energy AC-side to grid

1064

Grid: Active energy taken by the grid (energy produced by house)

Total DC power (sum of all PV inputs)

1066

Solar panels: Active power (all strings)

Total DC PV energy (sum of all PV inputs)

1056

Solar panels: Active energy (all strings)

Actual battery charge/discharge power

582

Battery: Active power

Total DC charge energy (DC-side to battery)

1046

Battery: Active energy charged to battery

Total DC discharge energy (DC-side from battery

1048

Battery: Active energy discharged from battery

NOTE: This profile has been tested with the KOSTAL Plenticore inverter. For compatibility with other models, contact KOSTAL´s technical support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.