2508_Wiser_KNX

Types of Moments

There are three types of moments in the app:

Type of moments

Parameters

Editable in the app

Display

KNX Scenes

  • Created in ETS or eConfigure.

  • Linked to scene widget in Touch visualization.

  • Displayed, controllable, located in the Moments screen in the Automations tab.

No

  • No icons or edit options in the app.

  • Editable in ETS or eConfigure.

Controller Scenes

  • Created in the controller (using Configurator).

  • Centralized.

  • Mapping exists only between scene actions and KNX group objects.

  • Logic is evaluated in the controller.

No

Tap to display the controller scenes in the app (green icon).

Tap to hide the controller scenes in the app (black icon).

NOTE: The house icon is displayed even without available controller scenes. It is just not functional.

Moments

  • Created in the mobile app.
  • Composed of devices.

  • Stored and evaluated in the controller.

Yes

  • Custom icons and edit options displayed.

  • You can create and edit them in the app.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?