2508_Wiser_KNX

Create Automations

  1. On the Home screen (Home Screen), tap > Automations > at the bottom right of the Automations tab to open the automation creator.

  2. Name your automation and assign it an icon.

  3. In the next step, add a condition (Add Conditions – If), set up a schedule (Add Period – When), and assign an action (Add Actions – Then) to your automation.

  4. Tap Save in the top right of the automation creator.


Your new automation appears on the list in the Automations tab.

In the Automations tab, you can turn your automation off and on, edit it (Edit Automations), or delete it (Delete Automations).


NOTE: Make sure the combination of conditions (If), periods (When), and actions (Then) are physically possible and do not go against each other.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.