2508_Wiser_KNX

Widget Configuration

To control your device through the mobile application, you must properly configure the widgets in the Touch plugin properly. The following sections describe which widget to use for the required functionality, the mandatory parameters, and group objects that need to be configured.

Function

Widget

Lighting

Light switch

Dimmer

Dali

RGB

RGBW

Shutters

Blinds

Vertical shutters with slats

Horizontal shutters with slats

Climate

General switch

AC switch

Thermostat + mode + fan

Thermostat VDC

Electric underfloor heating

Energy

Socket

EVlink Pro AC: This widget is set up through the Energy plugin, not the Touch configuration.

Safety

General alarm

Smoke alarm

Gas alarm

Water leak alarm

Multisensor

Weather station

Security

Door sensor

Window sensor

Motion sensor

Smart lock

Scenes

Scenes

Content

Content widget

Info

Info widget

NOTE: If you are adding a new widget that you want to control from the mobile app, use the App compatible filter, and you will see only those widgets that are compatible with the mobile application.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.