2508_Wiser_KNX

Notifications

On the Notifications screen, you can enable notifications and alarms.


Possible Settings

There are three setting options:

  • Enable notifications – enable or disable notifications. If you turn off notifications, you will not receive any notifications from the controller (alarms) or Schneider notifications (e.g., cloud outage).

    NOTE: If you enable notifications, you will be prompted to accept your consent to share personal information with a third-party notification service provider. You will not receive any system, device, or service notifications if you decline this consent. For more information on granting consents, see the Consents chapter.

  • Alarms – enable or disable alarms

  • Devices – set notifications for the devices (the whole device group or one by one):

    • Alarms

    • Events (low/critical battery level)

NOTE: Enabling/disabling notifications is related to the user's phone, not the controller. One user's notification settings do not affect the other user's notification settings.


Set Up Notifications

You can set notifications for the devices as follows:

  1. Tap > Notifications > Devices > select your controller from the Home management list.

    NOTE: The name of the specific controller that sent the notification is displayed in the notification's text.

  2. You can set up notifications for the whole group of device types or separately for each device from the group.
  3. For the whole group of the devices, just slide the button for the device type to the right, and all the devices of that type will start to send notifications.
  4. If you want to choose devices individually, tap the > icon at the end of the device group line and enable notifications by sliding the switch to the right for each device.
  5. Scroll down and enable/disable battery level notifications for your devices (Critical battery level and Low battery level swipe-toggle): Follow steps 3 and/or 4.



Message Center

Notification information display on the Message center screen.

The icon at the top right of the Home screen indicates new messages.

  1. Tap , and the Message center screen with the list of notifications opens.

    NOTE: Only the last notification displays for the device enabled to trigger notifications. Once the new notification arrives from your device, it replaces the previous one.

  2. Select the controller for which you want to display notifications (tap All controllers or Current controller)



Delete notifications:
Swipe your notification left > tap to confirm.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.