2508_Wiser_KNX

Moments

Moments allow you to change the state of several devices with a single tap. To create and edit moments, follow these steps:

  1. On the Home screen (Home Screen), tap .

  2. Select the Moments tab.

NOTE: A moment only sets the status of devices. If you want to revert the affected devices to another status, you must change it manually or create a reversing moment.


IMPORTANT: If you manually modify the moments from the controller, allow approximately 1 minute for the changes to propagate, then refresh the screen on your mobile application.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.