2508_Wiser_KNX

Add Moments

  1. On the Home screen (Home Screen), tap > tap at the bottom right of the Moments tab to open the moment creator.

  2. Name your moment and assign it an icon.

  3. Tap Add actions and select the devices you want to add to your moment > tap Done.

  4. Tap on each device in your action list and set its behavior (for example, plugs on, lights off, heating at 21 degrees) on the control screen.

  5. Tap Set at the top right of the device control screen.

    Repeat for all devices.

    NOTE: All devices are in their current state.

  6. Once you have set the properties of your moment, tap Save in the moment creator.


    You can add any device in your home. For your convenience, you can also filter the devices by room.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.