2508_Wiser_KNX

Mapping Energy Data to Energy Groups

Once the Energy plugin is installed in the controller, the energy data needs to be mapped to the energy groups to get them visible in the mobile application.
See more in Energy Plugin Installation/Update.

Back up your system after the configuration of all required equipment items. 

Back up after each energy configuration update.


The following image illustrates the flow of energy in your home:


Important:

The Energy section will only be displayed in your app when you have configured at least the GRID and a minimum of one additional load in the Energy plugin.

A section called Energy is created in the controller under the Trend logs tab for each energy equipment, where trend logs are automatically stored. Data is reloaded from these logs in case of an internet outage. However, if the internet outage lasts longer than 12 hours, the data cannot be reloaded and will be lost. Trend logs in the controller are read-only and cannot be deleted by the user.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.