2508_Wiser_KNX

Weather Panel

You enable the Weather Panel during the final step of the registration process (Create Your User Account) or in the Settings.

The Weather Panel displays weather data at the address you enter in the Home Management section (Home Management).

To view the weather information on your Home screen, follow these steps:

  1. Tap > Home screen > Weather Panel > enable Show Weather Panel.

    NOTE: Logging out of the application will clear this user setting. When you log back in, you must re-enable the Show Weather Panel feature.
  2. Tap Temperature units and select °C or °F.

  3. If you enable Use online weather service option, you will be prompted to provide consent to share your device's location. Granting consent is a prerequisite for this service to function.

    NOTE: The online weather service is a third-party service that provides weather forecasts based on your location. For more information on setting consents, see the chapter Consents.

  4. If you have a weather station (or more than one) in your KNX installation linked to a widget in your Touch visualization, you can select it here. Enable Use weather station information and select your weather station.


NOTE: Enable the weather information from your weather station in the installation, and the application replaces the data from an online weather service provider with the data provided by your weather station.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.