2508_Wiser_KNX

Add Actions – Then

Select one or more actions for your automation. We recommend defining up to 20.

You can also set delays between them.


There are four types of actions:

  • Run the device

  • Add a delay

  • Moment

  • Send notification


In the automation creator, tap Then tab > Add an action > select:

  • Run the device > select your device > tap Set delay > select the time of your delay > tap Save > tap Set.

  • Add a Delay: In the device control screen, tap Set delay > define a delay (mm: ss) > tap Save.

  • Moment > select from the list of moments > tap Done.

  • Send notification > tap Notify me. (You will receive a push notification when your automation is triggered.)

    NOTE: You must first enable receiving Notifications ( > Notifications > swipe-toggle Enable notifications to enable notifications).


You get back to the automation creator main screen.

NOTE: In a future release of the app, you will be able to send specific push notifications linked to the automation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.