2508_Wiser_KNX

Consents

Types of Consents

In the mobile application, there are two types of consent:

  1. Notifications consent: Each user can set this consent individually.

  2. Weather consent: Specific to each controller. The controller user can grant this consent to share the controller's location with the cloud weather service. Configuration is done for the active controller (the one selected on the Home screen).

First Start

When you log into the mobile application for the first time, you will need to handle your consent. Notification and weather consents work similarly. Upon being prompted, you can respond as follows:

Accept

The consent status changes to Granted.

Notifications: You will receive push notifications via the OneSignal service.

Weather: The weather forecast information based on your location will be displayed on the Home screen.

Decline

The consent status changes to Declined.

Notifications: You will not receive any push notifications.

Weather: The weather forecast data based on your location will not be available.

Close

The consent status remains Declined.

The consent will be in a pending state and displayed again at the next startup.

NOTE: You can only manage consents for the active controller in the mobile application if you have multiple controllers. Changes to consents or prompts for approval upon logging into the mobile application apply only to the active controller.

Consent Settings

If you decide to change the consent settings, follow these steps:

  1. Go to Settings > Account > Consents.

  2. Select the service you want to set the consent for and make the desired changes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.