2508_Wiser_KNX

Rates

To track electricity costs over time, set a rate value per unit of electricity (kWh).

Based on the entered data, the application creates graphs of the cost of electricity over time (see Insights).

Flat Rate

After you choose Flat rate as the contract option (My Contract Options), go to the Rates section of the screen and set the amount charged per kWh as follows:

  1. In the Tariff > Electricity > Rates > tap at the Flat Rate.

  2. Enter the amount per kWh.

  3. Tap Add.

The rate you set will appear in the Rates section on the Electricity screen. You can edit it from there: Tap > edit your rate > tap Update.

Time of Use (Peak/Off-Peak Hours)

If you choose Time of use as the contract option, define the subscription type as follows:

  1. In the Rates section, tap at the Peak Rate.

  2. Enter the amount per kWh.

  3. Tap Add.

  4. After defining all the rates, set up the schedules to specify which days of the week and times those tariffs apply:

    • Go to the Schedules section.

    • Tap Add a schedule.

    • In the Edit schedule screen, fill in the name of your schedule, select the rate to which it applies, and set the start/finish time and the days of the week.

    • Tap Save.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.