2508_Wiser_KNX

Live Tab

In the Live tab, you can monitor real-time energy consumption across your installation, including household appliances and other connected devices. It helps you monitor consumption patterns, identify high-usage devices, and understand how energy flows through your system.

Power Flow Overview

The power flow is visualized as a circular meter, showing the total current power consumption of your home in watts. At the top of the screen, you will see the available energy sources – based on your system configuration – along with the amount of energy each source is currently producing or consuming.

  • Grid consumption (kW): Indicates the current power drawn from the utility grid.

  • Battery usage (kW): Shows the current power drawn from battery storage. Visible only if a battery system is present.

  • Solar Production (kW): Displays the current power generated by your solar panels. Visible only if a solar energy system is configured.

  • Grid export: Represented by an outward-pointing arrow when energy is being fed back to the grid. Visible only if grid export is supported and active.


Each energy source is color-coded for clarity:

  • Grid – blue

  • Battery – dark grey

  • Solar panels – light green

  • The energy sold to the grid – dark green

Top Energy Consumers

Below the power flow, the app highlights the three household appliances with the highest current consumption (in watts). All other devices are grouped under Other loads.

Daily Energy Summary

Further down, you will find tiles summarizing your energy data for the current day (based on your configuration):

  • Consumption total (kWh): Total energy consumed in your installation.

    NOTE: Battery charging is excluded from house consumption.

  • Solar production (kW): Displays the current power generated by your solar panels. Visible only if a solar energy system is configured.

  • Self-sufficiency (%): The percentage of your total consumption covered by solar production and battery storage.

  • (%) of production used: The portion of your solar production that was consumed within your installation.


Hourly Energy Graph

At the bottom of the screen, a graph displays your hourly energy consumption, broken down by source:

  • The energy provided by the grid.

  • The energy provided by the photovoltaic.

  • The energy used from the battery.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.