2508_Wiser_KNX

Thermostat with Operation Modes and Fan

CONTROLLER

Settings

General tab

Mandatory fields

Optional fields

Title

Setpoint minimum value

Setpoint maximum value

Hide from mobile app and all other remote services (checkbox)

Fan step 1 – 6

Voice control (checkbox)

Thermostat title

Dewpoint alarm title

Setpoint step

Auto mode override on value (0-255)

Auto mode override off value (0-255)

Use custom operation modes (checkbox)

  • Mode name
  • Mode value

  • Mode status


Objects

Mandatory fields

Description

Optional fields

Description

Current temperature

Currently measured temperature for the widget (input value)

DPT_Value_Temp (9.001)

Operation mode input

Operation mode that widget writes by default when following icons are used:

  • Icon 1 = value 1

  • Icon 2 = value 2

  • Icon 3 = value 3

  • Icon 4 = value 4

DPT_1-byte unsigned int (05.010)

Current setpoint temperature output

Output value changed by the widget

DPT_Value_Temp (9.001)

Thermostat status, alert

1-byte status object interpreting values:

  • Bit 0: Comfort

  • Bit 1: ECO

  • Bit 2: Night mode

  • Bit 3: Frost/heat protection

  • Bit 4: Dewpoint alarm

  • Bit 5: Heating/cooling

DPT_1-byte unsigned int (05.010)

Current setpoint temperature input

Input value changed by external device (feedback field)

DPT_Value_Temp (9.001)

Switch on/off thermostat

Control object for thermostat on/off

DPT_Switch (01.001) or DPT_1-bit (01.0)

   

Switch on/off thermostat status

Feedback object for thermostat on/off

DPT_Switch (01.001) or DPT_1-bit (01.0)

   

Thermostat HVAC status

Feedback object; values correspond to the operation mode input.

DPT_1-byte unsigned int (05.010)

   

Heating/Cooling

Control object to control heating/cooling (1-bit)

DPT_1-bit (01.0)

   

Heating/Cooling status

Feedback object (1-bit)

DPT_1-bit (01.0)

   

Frost alarm

Feedback object (1-bit)

DPT_1-bit (01.0)

   

Dewpoint alarm

Feedback object (1-bit)

DPT_1 bit (01.0)

   

Battery level

Optional feedback object

DPT_Scale (05.001)

   

Battery alert

Optional feedback object

DPT_1-bit (01.0)

   

Is Active

System is actively heating/cooling

DPT_1-bit (01.0)

   

Device status object

Optional feedback object

DPT_1-bit (01.0)

   

Fan speed

Control object to control fan speed in %

DPT_Scale (05.001)

   

Fan speed status

Feedback object for the widget

DPT_Scale (05.001)

   

Fan manual mode

1-bit control object:

  • 1 = manual

  • 0 = auto

DPT_Switch (1.001)


Touch widget

Thermostat

Thermostat Danfoss


MOBILE APPLICATION

App widget

Control screens

Mandatory fields only

Mode, fan, and switch on/off control configured

Mode, fan, switch on/off and heating/cooling control configured

CONTROL SCREEN ELEMENTS


Current temperature

  • Displayed at the top of the screen.

  • The value is read directly from the KNX datapoint.

  • Units are shown in either °C or F, depending on system settings.


Status icon – Heating/Cooling

  • A dynamic icon indicates the current operating state.

  • The icon changes based on the relationship between the current temperature and the setpoint, and the selected mode:

Condition

Mode

Icon

Current temperature > Setpoint

Cooling

Current temperature > Setpoint

Heating

Current temperature < Setpoint

Cooling

Current temperature < Setpoint

Heating


Setpoint temperature

  • Displays the current target temperature.

  • The value is read from the datapoint.

  • Shown in °C or °F.


Mode button

  • Displays the currently active mode (e.g., Comfort, Eco, Night).

  • Tap the mode icon to open the mode selection screen.


  • Select the desired mode and tap Set to confirm.


Fan button

  • Displays the current fan status:

    • ON (with selected mode)

    • OFF

    • Auto

  • Tap the fan icon to open the fan mode selection screen.


  • Select the desired fan mode and tap Set.

  • To turn the fan off, deselect the currently active mode.


Cooling/Heating toggle

  • A simple toggle button that switches between cooling and heating modes.


On/Off button

  • The On/Off button controls the overall state of the thermostat. It turns the RTU (room temperature unit) on or off. This button does not control any actuator directly; instead it disables the logic inside the actuator, which stops the RTU from functioning.

  • When the button is ON, all interactive elements (buttons, sliders) are active.

  • When the button is OFF, the widget becomes inactive and settings cannot be changed.

  • The On/Off button can be mapped to control other functions, such as heating/cooling. For example, if it is mapped to air conditioning (heating/cooling), switching it OFF will stop the AC until it is turned back ON.

  • Even when the On/Off button is set to OFF, the Follow schedule and Manage schedule features continue to work as usual.

    NOTE: This feature is only available in the generic thermostat. It is not supported for the Danfoss thermostat or the VDC thermostat.

Custom Modes

The thermostat allows you to configure up to six custom modes, which extend the functionality beyond the standard modes like Comfort, Standby, or Sleep. These custom modes are useful for tailoring the thermostat’s behavior to specific user needs or scenarios.

Each custom mode must include:

  • A unique name – used to identify the mode in the app.

  • A mode value – the value sent to the system when the mode is activated.

  • A mode status – a status value that is used for feedback or logic in the system.

Adding and Managing Modes

  • To add a new mode, click the Add another mode button.

  • Fill in the Mode name, Mode value, and Mode status fields.

  • To remove a mode, click Remove this mode next to the specific mode you want to delete.

Using custom modes is optional – they are enabled by checking the Use custom modes box in the thermostat General settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.