2508_Wiser_KNX

EVlink Pro AC

For the EVlink Pro AC charger, the following registers shall be mapped to KNX objects:

Modbus register

Modbus address

Designation

OCPP Status

150

Status

Set Point

4003

Charging set point

Power Active Phase TOT

3059

Power

Energy Active TOT

3203

Energy

Set command

4001

Remote command

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.