2508_Wiser_KNX

Dimmer

CONTROLLER

Settings

General

Objects

Mandatory fields

Optional fields

Mandatory fields (per channel)

Optional fields

Title

Slider status wait time (s)

Voice control (checkbox)

Value object

Status feedback value object

Switch object

Status feedback switch object

Device status


NOTE: Multi-widgets can have different names for each of their loads. In the app, each channel will display as a separate widget with the name assigned.

It is recommended that multi-widgets be configured for only one device/load.
For example, if you have five lights, configure five multi-widgets – one multi-widget for each light.

Touch widgets

Rotary dimmer

Horizontal dimmer

Vertical dimmer


MOBILE APPLICATION

App widget


Control screen

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.