2508_Wiser_KNX

Schedules

You can set up schedules that determine specific times when a device changes its state.

These Schedules can be created and edited directly from your device control screen.

To access your device schedules:

  1. Navigate to the device control screen.

  2. Tap Manage schedules at the bottom of the screen to view the list of available schedules for your device:

IMPORTANT: If you manually modify the schedules from the controller, allow approximately 1 minute for the changes to propagate, then refresh the screen on your mobile application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.