2508_Wiser_KNX

Feed-in Tariff

If you use or sell energy from solar panels, with the Feed-in tariff function, you can track how much money you save by feeding energy into the grid and using your electricity produced from solar panels.

Set the Feed-in tariff as follows:

  1. First, set the Energy taken by grid from house parameter in the energy plugin of your controller:
    In the web browser, log in to your controller > energy plugin > Objects tab of the grid settings (Grid).

  2. In the mobile application, set the electricity sales rate:
    Click > Tariff > Feed-in Tariff > enter the Feed-in Rate > click Save.

Once you have finished setting up the Feed-in Tariff, you will see My savings in the Energy costs section ( > Insights > My annual bill).


My savings is the sum of the following items:

  • Production sold = your earnings for selling energy.

  • Production used = energy costs if you buy energy instead of your production (calculated according to your tariff).


If you click My savings, you can see the Savings and earning history chart with Production sold and Production used details for the selected period.


At the bottom of the screen, you see Production used by equipment. There is each energy equipment that uses the energy from your production sorted from the highest consumption to the lowest. The number shows the percentage of the total production consumed by the equipment during the selected period.


You can select a column from the chart to see
My savings
,
Production sold,
Production used, and
Production used by equipment
for the exact period (day/month/year).


Click Production sold and Production used to filter the earning history chart.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.