2508_Wiser_KNX

Subscription Type

The subscription type represents the interval and payments in the selected currency according to your energy supplier contract.

The Subscription Type option is available on the Electricity screen after you select the rate (see My Contract Options).

Example:

Your contract states a monthly advance payment of a certain amount in EUR.

  1. In the Tariff > Electricity > Subscription Type, check the Monthly interval and type the amount of money from your contract in the Subscription price field.

  2. Tap Save.

NOTE: The currency will be set automatically according to the country you set in your account. See User Profile.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.