2508_Wiser_KNX

Energy Plugin Installation/Update

You have to install the Energy plugin to the controller before the start of energy data mapping.

Install as follows:

  1. In your web browser, open your controller environment > click the cart icon to open Marketplace.

  2. Search for the Energy plugin > click next to the plugin > click Yes to install it.

  3. When the plugin icon appears on your controller's landing page, the installation is complete.

Follow the same procedure when updating your Energy plugin.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.