2508_Wiser_KNX

Cloud Connectivity

Firmware (Firmware Update) automatically installs the Cloud connector, KNX IoT 3rd Party API, and Touch visualization plugins in the controller, together with a new feature that allows the automatic updating of the plugins.


It is highly recommended that you enable automatic updates.

Then you do not have to manually update the plugins in your controller Marketplace in the future.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.