2508_Wiser_KNX

Add Schedules

  1. On the device control screen (Device Control Screen), tap Manage schedule.
  2. Tap at the bottom-right to add a new schedule.
  3. Enter a name in the text field, add a note, and set a period: yearly, monthly, or daily.
  4. Set the device state (On/Off, Open/Close).


    NOTE: Schedules apply to single devices only. If you want to trigger multiple devices simultaneously, create an Automation.

  5. Activate your schedule immediately by swiping the Activate schedule toggle.
    NOTE: You can activate or deactivate your schedules later as needed.

  6. Tap Create, and your new schedule will appear on the device´s schedule screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.