2508_Wiser_KNX

Light Switch

CONTROLLER

Settings

General

Objects

Mandatory fields

Optional fields

Mandatory fields (per channel)

Optional fields (per channel)

Title

Light 1 – 6 Title

Light 1 – 6 voice control enabled (checkbox)

Switch object

Status feedback object

Device status

NOTE: Multi-widgets can have different names for each of their loads. In the app, each channel will display as a separate widget with the name assigned.

It is recommended that multi-widgets be configured for only one device/load.
For example, if you have five lights, configure five multi-widgets – one multi-widget for each light.

Touch widget

Light switch

MOBILE APPLICATION

App widget


Control screen

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.