2508_Wiser_KNX

Vertical Blinds

CONTROLLER

Settings

General

Objects

Mandatory fields

Optional fields

Mandatory fields (per channel)

Optional fields

Title

Slider status wait time (s)

Height position

Status feedback for height

Movement object

Stop object

Device status


Touch widgets

Rotary shutter

Vertical shutter


MOBILE APPLICATION

App widget


Use the above optional objects for additional Up/Down buttons to control the blinds. You can also stop the movement by pressing and holding any of these buttons.


Control screens

  With optional objects
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.