2508_Wiser_KNX

Smart Lock

CONTROLLER

Settings

General

Objects

Mandatory fields

Optional fields

Mandatory fields

Optional fields

Title

Door control: Sends command to lock or unlock the door.

DPT_1-bit (1.001 Switch)

Lock state: Indicates the current lock status. Values:

  • 0 = JAMMED

  • 1 = LOCKED

  • 2 = UNLOCKED

DPT_8-bit unsigned value (05.)

Battery: Reports the battery level.

DPT_8-bit unsigned value (05.)

Door state: Indicates the current door position or error state. Values:

  • 0 = OPENED

  • 1 = CLOSED

  • 2 = JAMMED

  • 3 = FORCED OPEN

  • 4 <= UNSPECIFIED

DPT_8-bit unsigned value (05.)

NOTE: The following smart locks have been tested: YDM7116A, YMI70A, YDM3109A, and Kyra Pro (Yale).

Touch widget

Smartlock

     

Locked

Unlocked

Jammed

Forced open

MOBILE APPLICATION

App widget

Control screens

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.