2508_Wiser_KNX

Widget-Based Visualization

As an open standard for home automation, KNX guarantees the interoperability of the devices regardless of manufacturer.

The system integrator installs and configures the KNX project and creates a widget-based visualization with the KNX/Zigbee devices in the Touch plugin.

The Touch visualization is then converted to the visualization in the mobile app (as explained in Touch 3 Visualization).


In the Touch visualization, you can add your devices and change their parameters.

You can add other elements at any time later.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.