2508_Wiser_KNX

Edit Moments

Go to the Automations screen ( ) > Moments:

  1. Tap in the moment tile.

  2. In the Moment editor, you can:

    • Change the icon

      of your moment.
    • Change the name.

    • Change the desired state of a device (tap the device to open the device control screen).

    • Add more devices to the moment (tap Add actions).

    • Remove a device from the moment (swipe the device left and tap ).



  3. Tap Save to save the changes to your moment.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.