2508_Wiser_KNX

Delete Energy Data

You can delete data related to your house's and energy equipment's energy consumption. The option to Delete energy data is visible only when you are the owner of the controller and have the Energy plugin installed.

To delete your energy data, follow these steps:

  1. Tap > Account > Delete energy data.

  2. Before proceeding with data deletion, consider the following:

    • You are about to delete your house's energy consumption and energy equipment data.

    • This operation is irreversible. Once the data is deleted, it cannot be recovered.

    • By tapping Delete my energy data, you confirm your understanding of the consequences and agree to initiate data deletion.


  3. If you still want to proceed, tap Delete my energy data > type your password to confirm account deletion > tap Confirm.

    NOTE: If the password is incorrect, you will need to re-enter the password or cancel the process.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.