2508_Wiser_KNX

Firmware Update

  1. Go to www.se.com.

  2. In the top left corner, choose your country.

  3. Enter LSS100100 in the search bar. From the search results, choose LSS100100 Wiser for KNX logic controller.

  4. On the product page, scroll down to the Software and Firmware section.

  5. Click the firmware file (the highest available version) corresponding to your hardware version. It automatically downloads to your local repository.

  6. In your controller, access the Configurator (accessible only with the Admin account).

  7. Click ˃ System tab at the top left ˃ Upgrade firmware.

  8. In the pop-up window, click Choose File and select the file downloaded in step 3.

  9. Click Open and update the firmware. Once done, your controller automatically reboots.


NOTE: The Wiser KNX app is compatible with version 2 and higher hardware.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.