2508_Wiser_KNX

Floors & Rooms

In the Floors & rooms section, you can view all the rooms in your home either as a simple list or by enabling the Show floors level feature. This will display the rooms grouped by the floors you have assigned them to in the Touch visualization. You can rename the rooms and floors as you like and change the order in which they appear.

  1. Accessing floors and rooms:

    • Tap at the top right of the home screen > navigate to the Floors & rooms section in your application.

  2. Viewing rooms:

    • By default, all rooms are displayed as a simple list.

    • To view rooms grouped by floors, enable the Show floors level feature.

    • When Show floors level is enabled, rooms are grouped by floors not only on the Home screen, but also on the Select devices screen when creating automations and moments.

  3. Customizing names:

    • You can rename any room or floor to suit your preferences better.

    • Click on the name of the room or floor you wish to change > tap .

    • Enter the new name > tap Save.

  4. Reordering rooms:

    • You can change the order in which rooms are displayed.

    • Make sure the Show floors level option is disabled.

    • Tap > drag and drop the rooms to the desired position.

    • Tap Save.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.