2508_Wiser_KNX

Touch 3 Visualization

Touch 3 is a plugin that provides a widget-based visualization and allows you to control or read information from devices in your installation (KNX, ZigBee, Modbus, BACnet), as long as they have been integrated into the controller and their group objects have been mapped accordingly. It also provides input for the mobile application. With the Touch Config plugin, the system integrator designs the visualization.

Creating Touch 3 Visualization

  1. On your web browser, log in to your controller.

  2. On the Start page of your controller, click Touch Config to open the visualization configurator Main screen.

    NOTE: When you first open the Touch Config, at least one floor is already present by default.
  3. To add more floors (if needed), click ADD NEW FLOOR at the bottom of the page, name your floor, and press Enter on your keyboard.

  4. Continue by adding rooms: Click ADD NEW ROOM, name your room, and press Enter on your keyboard.

  5. Assign icons to your rooms: Open the room and click ICON.

    Icons are categorized in several tabs:

    • SVG

    • Title

    • Line Awesome

    • Custom

    Each category has a different style. Custom icons can be uploaded.

  6. Add widgets to your room:
    • Click the + icon in the upper right corner of the room screen.

    • Select the widget you want to add.

  7. In the widget Settings dialogue:

You can copy rooms together with all widgets and paste them into any floor of your building. The room and widget styles are preserved.

The KNX objects mapping has to be changed according to your installation.

Learn more on creating Touch visualization: https://www.se.com/ww/en/download/document/AN002_105_SL/.

Widget Verification

When creating widgets, ensure all required fields for each widget are entered as described in the following pages. Before saving the widget, you can perform the following verifications:

  1. Verify for Local

    • Click the Verify for Local button. This verification ensures that all required fields for controlling the widget from the Touch visualization are filled.

    • If everything is correct, you will see the green message Verified for Local at the bottom left of each Settings dialogue tab.

    • If any mandatory fields are missing, they will be highlighted in red for you to fill in.

  2. Verify for App

    • Click Verify for App. This verification ensures that all required fields for controlling the widget from the mobile application are filled.

    • If everything is correct, you will see the green message Verified for App at the bottom left of each Settings dialogue tab.

    • If any mandatory fields are missing, they will be highlighted in red for you to fill in.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.