2508_Wiser_KNX

Home Management

You can have more than one home linked to your app account and add additional accounts for other people so they can access your home.

For example:

Second residence

If you have a second home and want to avoid having different accounts to access it (Adding New Home).

Family sharing

Each family member can create an account so the parent does not have to share their credentials (Enable Access to Your Home).

SpaceLogic KNX Remote

Homeowners can enable permanent or time-limited remote access (Enable Access to Your Home).


There are two options how to access the Home Management section:

  1. Tap > Home Management > select the home you want to manage.

  2. On the Home screen, tap your home name at the top center of your screen > select from your homes or tap Home Management.


If you tap on your home in the Home Management section, you can:

Edit your home name

Tap your home > tap > edit the name > tap Confirm.

Edit the address

Tap your home > tap Home address > type the address > tap Next > tap Submit.

Remove/unlink home from your account

If you are a Homeowner: Tap your home > tap Remove Home > Confirm.

If you are a user: Tap your home > tap Unlink me > Confirm.

Manage access

Tap your home > tap Manage access > select the access request you want to manage > edit parameters (Role, Access period, Remove access) > tap Update access/Remove access.

Manage remote access via VPN

These options are only visible if:

  • You are the Owner of the selected controller, or

  • You have Admin or System Integrator access.

If your access level is Family, the screen will appear in its standard form without these options.

Refer to Managing Remote Access via SpaceLogic KNX Remote Service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.