2508_Wiser_KNX

Typical User Scenarios

These scenarios may typically occur in real installations (the list is not exhaustive):

Scenario

Action

1. A user wants to stop monitoring a household appliance (e.g., a washing machine) and wants to remove it from history.

An installer deletes the respective equipment in the Energy plugin. By doing so, the historical data will be deleted forever. 

2. A user wants to stop monitoring a household appliance (e.g., a washing machine) but wants to preserve its history.

An installer deletes the power and the energy - the KNX objects of the respective equipment.

3. A user decides to replace the monitoring of one household appliance (e.g., a washing machine) with another (e.g., a dryer) using the same energy meter (e.g., smart socket). 

An installer physically disconnects the monitored household appliance and connects the other household appliance. Then the installer creates new Energy consumer equipment and maps the respective KNX objects.

If a user wants to preserve the history of the recently monitored household appliance, follow Scenario 2; otherwise, follow Scenario 1.

4. An energy meter linked to monitored equipment is broken down and needs a replacement.

An installer replaces the damaged energy meter and commissions a replacement meter to the controller.

In the Energy plugin, the installer maps KNX objects of the new energy meter to the monitored equipment.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.