2508_Wiser_KNX

EVlink Pro AC

CONTROLLER

Settings

General

Objects

Mandatory fields

Optional fields

Mandatory fields

Optional fields

Title

Equipment type

Charger type

Rooms

Power limit (A)

Reverse direction

Status

Consumed on last charge

Remote command

Energy

Power

EV state

Charging set point

Charging start

Charging stop

Transaction time

Device status

Important charging instructions

  1. Starting charging: When charging begins, you have two options:

    • Pause: You can pause the charging process.

    • Stop: Alternatively, you can stop it.

  2. Paused charging: If you choose to pause charging:

    • You can later resume it.

    • During the pause, you cannot disconnect the car from the charger (the cable plug remains locked in the charger socket).

  3. Stopped charging: If you decide to stop charging:

    • You must unplug and then re-plug the car before initiating charging again.

NOTE: After charging is complete, it may take up to 15 minutes to synchronize information and reset the app charge counter. If you start charging again, the counter will likely use values from the previous session as a starting point. The counter will display accurate values once the charging level exceeds the prior session's.

Status of the charger

Meaning

EVlink Pro AC / Available

EV is unplugged.

EVlink Pro AC / Loading

EV is plugged in, but charging has not started.

EVlink Pro AC / Charging

EV is charging.

EVlink Pro AC / Paused by EV

Paused by the EV.

EVlink Pro AC / Paused by user

Paused by the user or the EV charger.

EVlink Pro AC / Finishing

Charging has been stopped, and the EV is still plugged.

EVlink Pro AC / Error

An error has been detected.


Widget

This widget is set up through the Energy plugin, not the Touch configuration. See Electric Vehicles.

EVlink Pro AC


MOBILE APPLICATION

App widget


Control screen

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.