2508_Wiser_KNX

Home Screen

The Home screen offers a comprehensive view of all the devices in your home. Here are the key features:

  1. Device Status: Quickly check the status of your devices.

  2. Device Control: Easily manage and control your devices directly from the Home screen.


Home screen overview:

Weather panel

Weather

Location

Humidity

Wind speed

Temperature

Time of the sunrise and sunset

Moments

Tap the moment tile to trigger the moment without navigating to the Automations screen. In the Settings section, you enable the display of moments on the Home screen.

Favorites

Displays items that you have marked as favorites.

All

List of all rooms with the devices

Rooms – quick access

Rooms and devices management.

Drag to scroll through the rooms and their devices.

Home screen icon

Tap to show the Home screen

Automations

Tap to navigate to the Automations screen, to set up Moments and Automations.

Message center

Tap to see device notifications and system messages.

Energy

Tap to manage and monitor the consumption and use of energy from the various sources available in your home.

Settings

Account

Tariff

Floors & rooms

Devices

Notifications

Home management

Home screen

Support

About

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.