2508_Wiser_KNX

Wiser KNX System

The Wiser KNX system provides a robust, convenient, and scalable solution for managing your KNX installation.

You can integrate it with the new Wiser KNX mobile application if the app is available in your country (see Wiser KNX App Availability).

The Wiser KNX application lets you control and monitor your KNX and ZigBee devices from anywhere with an Internet connection.

Additionally, the Wiser for KNX logic controller (LSS100100) serves as a versatile multi-protocol logic controller, allowing you to:

  1. Visualize your KNX installation

  2. Control your KNX and ZigBee devices

  3. Create advanced logic

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.