2508_Wiser_KNX

My Contract Options

To track your energy consumption costs, start by choosing the type of contract you have with your supplier.

On the Electricity screen, under My contract options, tap one of the three types of contract at the bottom:

  • Time of use (peak/off-peak hours)

  • Flat rate

  • No contract (set by default)

If you choose Flat rate or Time of use (peak/off-peak hours), you have to specify the type of subscription and rates (see Subscription Type and Rates).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.