2508_Wiser_KNX

Prepare Your Controller

If you want to connect with the Wiser KNX app, you must enable your Wiser for KNX controller for cloud communication.

  • Update the firmware in your controller to the highest available version (Firmware Update).

  • Enable Cloud Connector and KNX IoT 3rd Party API plugins. Both will be automatically installed with firmware updates.

NOTE: It is recommended to allow automatic updates of Cloud Connector and KNX IoT 3rd Party API plugins.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.