PowerTag Modbus 1-phase
For PowerTag Modbus 1-phase energy sensor, the following registers shall be mapped to KNX objects:
|
Modbus register |
Modbus address |
Designation |
|
Voltage |
3020 |
RMS voltage |
|
Frequency |
3126 |
Frequency |
|
Current Lx |
- |
RMS current (channel X) |
|
Active Power Lx |
- |
Active power (channel X) |
|
Lx Active Energy Delivered |
- |
Active energy delivered (channel X) is the absolute energy accumulator when Active power has a positive value. |
|
Lx Active Energy Received |
- |
Active energy received (channel X) is the absolute energy accumulator when Active power has a negative value. |
|
Partial Lx Active Energy Delivered |
- |
A resetable register of Active energy delivered (channel X). |
|
Partial Lx Active Energy Received |
- |
A resetable register of Active energy received (channel X). |
|
Clear Energy |
6000 |
Write 21920 to clear all partial active energy registers. |
|
Power Factor Lx [-1,1] |
- |
Power factor in the range – 1 to 1 (channel X). |
|
Power Factor Lx [-2,2] |
- |
Power factor in the range – 2 to 2 (to indicate capacitive or inductive load, channel X). |
|
Lx Direction |
- |
Write 1 to change the active power direction (from positive to negative or vice versa, channel X). |
|
Lx CT |
- |
The current coil rate, only 80A is supported. |