2508_Wiser_KNX

Electric Underfloor Heating

CONTROLLER

Settings

General

Objects

Mandatory fields

Optional fields

Mandatory fields

Optional fields

Title

Floor heating title

Minimum value

Maximum value

Temperature alert threshold

Temperature alarm title

Setpoint step

Voice control (checkbox)

On/Off object

On/Off status object

Temperature object

Temperature status object

Temperature alert object

Touch widget

Floor heating

The On/Off button on the widget can be used in two ways:

  • To control a relay in the actuator.

  • To control the RTU of the floor heating system.


MOBILE APPLICATION

App widget


Control screen

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.