2508_Wiser_KNX

Mounting Your Controller

  • Check the instruction sheet.

    https://www.go2se.com/ref=LSS100100

  • Install your controller in the low-voltage electrical cabinet.

    It is powered by a 24 V power supply and connected to the KNX network through twisted pair (TP) cables or IP.

  • Connect your controller to the Internet router.

    Without the Internet, the controller cannot be controlled via the app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.