2508_Wiser_KNX

Automations

To use Automations in the mobile app, ensure the Automation plugin is installed in the controller. You can install the Automations plugin from the Marketplace. Enabling automatic updates is recommended so you always have the latest version installed.


Automations trigger devices automatically based on predefined conditions. Here are some examples:

  1. Sunrise scenario: If it is sunrise, automatically open the living room blinds.

  2. Weekend motion detection: If motion is detected on weekends between 9:00 and 17:00, prevent the lights from switching on.

To create and edit automations:

  1. Navigate to the Home screen (Home Screen).

  2. Tap .

  3. Select the Automations tab.

NOTE: In a future release of the app, you will be able to send specific Push notifications linked to the automation.


IMPORTANT: If you manually modify the automation from the controller, allow approximately 1 minute for the changes to propagate, and then refresh the screen on your mobile application.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.