2508_Wiser_KNX

Pair Your Controller

After creating your user account (Create Your User Account) and logging in (Logging in) for the first time, the app will welcome you and prompt you to pair your controller.

NOTE: If your controller is already paired with your account, you can skip this section.

Pairing Guide

  1. Start the Pairing Wizard

    Tap to begin.

  2. Prepare Your Setup

    • Make sure your controller is powered and properly connected.

    • Ensure your phone is on the same network as the controller.

    • Before pairing, it is recommended to manually force any pending updates. If the DNS is not set up correctly, available updates may not appear on the controller.

  3. Tap Next to continue.

  4. Update the Controller Firmware

    • Go to your controller and install the latest firmware from https://www.se.com (Firmware Update).

    • This firmware includes essential plugins: Cloud Connector, KNX IoT 3rd Party API, and Touch Visualization.

  5. Enable Required Plugins

    • Activate the Cloud Connector and KNX IoT 3rd Party API plugins.

    • It is recommended to enable automatic updates for these plugins.

  6. Check Your Visualization Setup

    • Ensure your controller has a Touch visualization with widgets organized into rooms (Touch 3 Visualization).

    • All devices should be correctly configured in their respective widgets.

  7. Reboot the Controller:

    After rebooting, tap Next in the app.

  8. Search for the Controller

    • Tap Search for the controller.

    • Select your controller from the list to start pairing automatically.

    • Alternatively, tap Enter manually , input the IP or MAC address, and tap Pair.

      NOTE: You can also scan the controller’s QR code. If scanning fails, enter the MAC address manually.

  9. Name Your Controller

    After pairing, give your controller a name and tap Next.

  10. Set Your Location

    • Allow the app to access your location or select it manually on the map.

    • The location helps provide local weather data. Tap Submit.

  11. Review and Confirm

    Check your details and tap Pair controller.

  12. Enable Weather Info (Optional)

    After pairing, you can enable the weather panel on your Home screen. This can be changed anytime in Settings.

  13. Use a Weather Station (Optional)

    If a weather station is detected, you can choose it as your weather data source. This setting is also adjustable in Settings.

After Pairing

Your controller is now paired and will appear at the top of the app’s Home screen.

To pair another controller later:

  • Go to the Home screen

  • Tap > Home Management > Pair new controller.

  • Follow the same steps in the wizard

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.