Access Type Default
To begin commissioning the controller using the Default access type, follow these steps in the UPLOAD tab:
-
Open the controller access settings:
In the UPLOAD tab, click Select controller access > choose Access type > Default.
This mode is used for local configuration only, where the controller is directly connected to your PC via an Ethernet cable.-
The eConfigure KNX tool communicates with the controller using the IP address 192.168.0.10.
-
Your PC’s IP address is automatically adjusted to ensure communication with the controller.

-
-
Switch to User-defined access:
After completing the initial setup in the Default mode, connect the controller to your local network (router), and switch to Access type > User-defined. -
Continue with User-defined configuration:
Proceed with the steps described in the Access Type User-defined chapter to complete the commissioning process.