260130_LSS900100_eConfigure_KNX_SW

My User Settings

User settings are default for all new projects. You can customize them:

  1. Click on the Menu button at the top left of the screen > click My user settings.

  2. Fill in the information:

    • Basic parameters

      • Company name

      • Application language

      • Product catalog for a country (allows you to display only the devices available in your country)

        NOTE: Select the correct catalog carefully, because you cannot change it later in the project.

    • Advanced parameters

      • Free spaces (%) – choose the available free space when using automatic composition.

      • Group address rules: If you select Structured scheme the directives of knx.org Switzerland are applied.

      • Enable advanced device parameters: This feature allows displaying advanced device parameters if they are available for the device.

      • Allow usage data collection: It is recommended to allow this feature. It helps us improve the software.

      • Restore user preferences: This feature allows you to restore the user preferences to default values.

        Export logs: This button allows you to generate a file containing projects and detailed logs of the software's activities and events. This file can be useful for troubleshooting, analyzing system performance, or providing information to technical support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.