260130_LSS900100_eConfigure_KNX_SW

System Requirements and Installation

Disk space

A minimum of 3.5 GB of free space on your disk is required for eConfigure KNX.

ETS application

eConfigure KNX Lite: The ETS application is included in the installation package. During the installation of eConfigure KNX Lite, the ETS software will automatically install the version tested with eConfigure KNX Lite. If ETS is already installed on your computer, it will be updated to the latest version, and your projects will be retained.

eConfigure KNX Expert: You need to download and install ETS separately before installing eConfigure KNX Expert from the my.knx.org online shop.

Catalog

eConfigure KNX Lite: The catalog is included in the installation package.

eConfigure KNX Expert: You need to download and install the catalog separately. The catalog is the same for both eConfigure KNX Lite and eConfigure KNX Expert and can be found on www.se.com.

Space Logic KNX Remote

To use Space Logic KNX Remote, you need to download Schneider Electric Remote Service and the Management application. (SpaceLogic KNX Remote).

When using eConfigure KNX, the ETS runs in the background of your computer (the ETS tab might appear in the Windows task bar).


eConfigure KNX Lite

Install the eConfigure KNX Lite software as follows:

  1. Go to www.se.com > type eConfigure in the search bar > select your the desired eConfigure KNX edition (for ETS 5 ot 6) > download it to your local storage.

  2. Download the corresponding eConfigure KNX (ETS5/6) Catalog.

  3. Launch the eConfigure KNX installation on your computer and follow the wizard.

  4. Install the eConfigure KNX catalog.

    NOTE: The catalog is not included with eConfigure KNX Lite and must be installed separately.

  5. If you want to do remote maintenance, install Schneider Electric Remote Service (refer to SpaceLogic KNX Remote).

Launch the software after installation and start to use it.

eConfigure KNX Expert

Install the eConfigure KNX Expert software as follows:

  1. Go to my.knx.org > purchase eConfigure KNX Expert > download it to your local storage.

  2. Launch the ETS software on your computer.

  3. ETS6: Go to Settings click Install app > select the installation file from your local storage > click Open.

    NOTE: In ETS5, click Apps on the right side of the bottom bar > click the plus sign to select the installer file from your local storage.

  4. Go to www.se.com and download the corresponding eConfigure KNX (ETS5/6) Catalog. The catalog is the same for eConfigure KNX Lite and eConfigure KNX Expert.

  5. Install the eConfigure KNX catalog.

    NOTE: The catalog is not included with eConfigure KNX Expert and must be installed separately.

  6. After the installation is complete, open the ETS software again, open an existing project or create a new one.

  7. ETS6: In your project, go to Panels > All panels > Schneider Electric > click eConfigure KNX Expert to launch it.

    NOTE: In ETS5, click Apps > click eConfigure KNX Expert.

  8. If you want to use Space Logic KNX Remote, install Schneider Electric Remote Service (refer to SpaceLogic KNX Remote).

eConfigure KNX Expert will launch as a new window in ETS and you can start to use it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.