260130_LSS900100_eConfigure_KNX_SW

Parameters

In the FLOOR tab, besides the catalog and scene module, there is also a PARAMETERS section. This section is used for setting up individual devices/loads.

Not all parameters of the devices are available in eConfigure KNX Lite. Make sure the functionalities you want are integrated into the software. Some typical examples are described further.

Follow the tutorials available on Exchange Community (https://community.se.com/) for more details.

Setting Parameters

To set parameters, select an item on the floor plan:

Adjust the behavior of the respective device/load in the PARAMETERS tab on the right.

Types of parameters:

  • Basic parameters: For example, simple lighting loads.

  • Advanced parameters: Such as push-buttons with display.

Enabling Advanced Parameters

Advanced parameters do not display automatically. You need to enable their visibility in the main menu:

  • Click at the top left of the screen > My user settings > Enable advanced device parameters.

Adjusting Advanced Parameters

If advanced parameters are available for a device, you can further adjust them by clicking next to the device name:

Not all parameters of the devices are visible by default:

  • Go to the Parameters tab of your device > click (Advanced device parameters) in the upper right > choose which parameters will be available for the device (check the Visible checkbox for each parameter).

Representation of Advanced Parameters

Each advanced parameter is represented by a channel shown as a dot next to the device icon.

In the PARAMETERS section, you can navigate through specific advanced parameters using the arrows below the device name and icon.

To work with an advanced parameter, it must be marked as "visible" in the Advanced device parameters dialog.

This device has 7 channels (= 7advanced parameters “visible”):

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.