260130_LSS900100_eConfigure_KNX_SW

Access Type User-defined

After completing the initial setup in Default mode, proceed with the Access type > User-defined to finalize the controller configuration over your local network.

Follow these steps in the UPLOAD tab:

  1. Switch to User-defined access:
    In the UPLOAD tab, click Select controller access > choose Access type > User-defined.

    NOTE: The controller must be reachable from your computer over the local network.

  2. Enter network details:
    Provide the controller´s IP address and the HTTPS port assigned to it.

    NOTE: Verify the HTTPS port in your controller settings.
  3. Lock the controller API:
    Use the Lock access function to secure the controller.
    eConfigure KNX will automatically unlock the controller for the duration of the upload.

    NOTE: For security reasons, ensure the API is locked again after your configuration is complete.

  4. Select Touch configuration settings:
    Choose how to handle the existing Touch configuration on the controller:

    • Replace: Deletes the current configuration and uploads a new one.

    • Update: Updates the configuration while preserving user changes made in Touch Config.

  5. Close the access settings:
    Click Close to confirm and exit the access configuration.

  6. Start the upload process:
    In the UPLOAD tab, go to the list of devices to configure (left side), select your controller, and click the arrow in the center of the screen to begin uploading.

  7. Confirm connection:
    When prompted with a Potential Security Risk dialog, click Trust to establish a secure connection to the controller.

  8. Follow the steps in the upload wizard.
    Complete the steps in the upload wizard. The controller may restart to apply IP changes. Ensure your PC´s network settings match the new controller IP.

  9. Click Close to complete the upload.

Once the upload is successful, the controller will appear in the list of configured devices on the right side of the UPLOAD tab.

IMPORTANT: After each VPN session, update the controller’s IP address to the correct User-defined value.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?