260130_LSS900100_eConfigure_KNX_SW

Bill of Materials (BOM)

The bill of materials (BOM) is a list of all devices of your project.

The USB interface is not included in BOM. You can use the same USB interface for all your project.


Verify that you set up your actuators and controllers properly. Otherwise, they will not appear in the list of hardware you generate from your BOM.

If your project has several line segments, please check whether the tab SWITCHBOARD > KNX Topology is correctly set.


The BOM contains only the devices. Do not forget to order additional accessories:

  • Push-buttons: frames, installation boxes, and additional accessories.

  • Controllers.


Each BOM item contains the following information:

  • Name

  • Reference

  • Description

  • Range

  • Color

  • Reference


To view the BOM, click in the upper right.


From the BOM, you can:

  • Export: group addresses, reports, and lists (for your customers and users).

  • Apply color to all products.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.